概要
現在、5Gをサポートするためにアップグレードと拡張が進められている4Gインフラには、超低遅延をサポートする新たなスイッチングテクノロジーが含まれます。これらのネットワークは、追加される超高周波ミリ波スペクトラムを組み込むために大幅に拡張されます。この2つの追加要素の組み合わせは、5Gの利点である高速伝送と高速データ・レートを可能にする基盤です。5Gインフラはまた、優れたパフォーマンスを実現するビームフォーミングアンテナアレイを運用することで、大規模MIMO技術を活用します。
5Gプロバイダーと関係者は、より高い周波数(10GHz以上)で複数の課題に直面しています。これらの高周波数信号は、木・壁・人などの障害物によってブロックされやすくなります。これを克服するために、マイクロセル、中継器、ビームフォーミングやビームステアリングのような伝送技術の使用など、より高い周波数の5Gシグナル用をより効果的に伝播するためのさまざまな戦略があります。これらのアプローチにもかかわらず、高周波数信号が信頼できなかったり、利用できなかったりする場所や時間帯があることに変わりはありません。このような場合、スマート5Gネットワークは、シームレスに別の周波数や帯域に伝送をリダイレクトします。
5Gインフラはセルタワーを超え、建築環境の奥深くまで到達する必要があります。マイクロセルは、ますます密集する都市インフラに浸透するために使用されます。これらの小規模送信機は、5Gで使用される高い周波数を拡張し、他の方法では届かない建物内デバイスに届きます。このようなマイクロセルが普及するということは、環境にシームレスに溶け込む必要があるということです。
伝送インフラから最終使用デバイスに至るまで、5Gのすべてのコンポーネントは、4Gではそれほど差し迫ったものではなかった課題に直面することになります。特に送電とアンテナに関しては、設計者は以下のような課題に直面することになります。
高周波アンテナアレイの製品設計への組み込み
5Gの典型的な高周波数に対する最適なコネクターと相互接続アプローチの発見
5Gデバイスの同軸およびアンテナ性能を最適化するための最適な材料とパッケージング戦略を知る
5Gアンテナのアンテナ配置のベストプラクティスの決定
モレックスは、設計者が大量生産に適した5G製品を作成できるように、製品とRFシステム製造の両方の専門知識を提供しています。デバイスに5G機能を設計するには、最適な5Gコンポーネントを選択するだけでなく、感度の高いRFアンテナやコネクターを適切に組み込む熟練したテクノロジーも必要です。
特集
注目の動画
Molex develops products that brings 5G to reality. 5G technology is connecting everything around us, our mobile devices, our streets, our vehicles, and our buildings - enabling communication at the highest speeds. 5G automotive technology enables direct communication between vehicles, while other 5G-enable applications include smart wearables, 2-way communication remote healthcare and advanced automated factories.
5Gソリューション
Mobile communication is an essential part of our daily lives and Molex produces products for the communications, datacom, IoT and automotive markets. 5G technology is being designed into game-changing applications such as wireless surveillance cameras, distance learning, and game streaming. 5G is also connecting vehicles, such as cars, commercial trucks, and farming equipment to the ever-growing 5G ecosystem.
5GおよびIoT